Installing the Examples Database

The Example Projects database is installed automatically as part of a Full installation or Typical Server and Clients installation.

The Example Projects database is automatically imported into your installation if there is no existing database present.

If an existing database is present, then the Example Project database files are copied to your system, but are not imported. You can import the Example Project database at a later date if required.

NOTICE

UNEXPECTED BEHAVIOR OF APPLICATION

The Example Projects database can only be installed at Root Group level within a database. It contains security settings, which might affect the configuration of an existing database.

We recommend that the Examples Project database be installed as a standalone server and used only for training and in conjunction with the Tutorial material.

Failure to follow these instructions can result in unexpected configuration changes.

If your installation choice for Geo SCADA Expert does NOT include the Examples Projects database as part of the installation you need to select a Custom installation (see Choose Setup Type) or import the Example Project database when your installation is complete. When you choose Custom on the Choose Setup Type ‘page’, the Custom Setup ‘page’ is displayed.

Use the ‘tree’ on the left-hand side of the ‘page’ to choose and expand the Server branch and locate the Configuration Samples component.

Right-click on the branch and select the Entire feature will be installed on local hard drive option. The selected component and all of its sub-components will be installed.

The Example Projects database is automatically imported into your installation if there is no existing database present.

If an existing database is present, then the Example Project database files are copied to your system, but are not imported. You can import the Example Project database at a later date if required.

When you have completed the installation of Geo SCADA Expert, (see Create a Super User Account), use the following procedure to complete the setup of the Example Projects:

  1. Check that the Geo SCADA Expert server is running. To do this, look for the Geo SCADA Expert icon in the Windows taskbar. The Geo SCADA Expert icon should be blue, like this:

    If the Geo SCADA Expert icon is a different color, this indicates a different server state (for more information, see The Server Icon).

    If the Geo SCADA Expert icon is not shown, the Server Icon application may not be running.

    In Windows, select the Start menu. Scroll down the alphabetical list of installed applications and expand the EcoStruxure Geo SCADA folder. Select the Server Icon option.
    The Server icon is displayed in the taskbar in Windows.

  2. Right-click on the Server icon and select the Start Server option.
  3. Once the Server is running, start ViewX:
    • Double-click on the ViewX desktop icon.

      Or:

    • In Windows, select the Start menu. Scroll down the alphabetical list of installed applications and expand the EcoStruxure Geo SCADA folder. Select the ViewX option.
  4. Once ViewX has started, log on to ViewX using the Super User account.

    For a new installation this is the only user available, see Super User Account.

    You can now Enable Example User Accounts.


Disclaimer

Geo SCADA Expert 2022