Display Current Trend
Associated with: Master station accumulators, and many types of point
Security permission required to access this option: Read
Select this option on the Object Menu to display a Trend of current data for the selected point or accumulator, starting from the current time. The Trend is updated as further values are received and processed (see Trends).
With a ViewX client on a Multi-Monitor Setup, you may be able to select the name of the Window Container in which to display or edit a document. Each Window Container displays on a particular monitor by default. Such options are only available when you select certain Display... or Edit... pick actions from the Database Bar or Operator Documents Bar. For more information, see Ability to Specify the Window Container in which to Display or Edit a Document.