Display Objects

Associated with: Groups, Group Templates, and Group Instances

Security permission required to access this option: Read

Select this option on the Object Menu to display a Queries List of the items that are in the selected Group, Group Template, or Group Instance (see Lists). The List will also include the database items that are in any Groups or Group Instances that are nested within the Group, Group Template, or Group Instance. Only the database items to which your User Account provides access are included in the Queries List.


With a ViewX client on a Multi-Monitor Setup, you may be able to select the name of the Window Container in which to display or edit a document. Each Window Container displays on a particular monitor by default. Such options are only available when you select certain Display... or Edit... pick actions from the Database Bar or Operator Documents Bar. For more information, see Ability to Specify the Window Container in which to Display or Edit a Document.

Be aware that if you have a Group Template nested within a Group, although the Queries List will include an entry for the Group Template itself, it will not include the contents of that Group Template. This is by design. To view a Queries List of the database items that are within a Group Template, use the Display Objects option on the Group Template itself (rather than from the Group in which that Group Template is nested).


Disclaimer

Geo SCADA Expert 2022