Configuring a WITS Analog Point

The Geo SCADA Expert WITS driver supports Analog Input and Analog Output points. These analog points have a combination of configuration settings that are:

To configure a WITS analog point, you need to use the DNP3 WITS Analog Input Point Form or DNP3 WITS Analog Output Point Form as appropriate.

WITS Analog Point Form - Alarm Limits Section

The Form contains many fields, organized into tabs. Some of these tabs are common to many types of database item, but the Analog Point contains settings that are specific to WITS.

The Control and Control Checks tabs are only available on the Analog Output Form. The Input tab is only available on the Analog Input Form.

For information on the settings on the various tabs, please refer to the following topics:


Disclaimer

Geo SCADA Expert 2022