Downloading Configuration Changes

In order for outstations or PLCs and their component parts—such as points—to communicate correctly with the ClearSCADA server, their database configuration has to be stored at the outstation. With devices with which ClearSCADA communicates using an advanced driver, you typically configure the properties of those items in the ClearSCADA database, and then write (download) the relevant properties to the outstation. (In those instances where advanced driver outstations do not support downloading, see the relevant driver-specific documentation.)

(Devices with which ClearSCADA communicates using simple drivers tend not to support downloading of configuration from a SCADA master. When configuring simple driver devices in ClearSCADA, ensure that the configuration in the ClearSCADA database replicates the settings that exist at the actual devices that those items represent.)

To download configuration to an advanced driver outstation, you use the Download Configuration pick action. The pick action is available if:

Outstations on some advanced drivers have the ability to indicate that they have no configuration, or that their existing configuration is corrupt. On receipt of such an indication, ClearSCADA can automatically download the relevant configuration to the outstation.

Be aware that changing an item’s configuration in the ClearSCADA database does not automatically initiate a download—you need to trigger such a download using the Download Configuration pick action.

The Download Configuration Required system color indicates when configuration changes have been made in ClearSCADA, which have not yet been downloaded to the relevant outstation.

While a download is in progress, you must avoid making any configuration changes to that outstation or any of its dependants. Once the download is complete, you can make further changes to the configuration if required—such changes will be flagged needing to be downloaded to the outstation the next time that a Download Configuration request is made.

An entry is added to the Events List whenever a request is made to Download Configuration to an outstation. The entry will indicate the success, or otherwise, of the request.

The Download Configuration pick action can download, where supported by the driver or outstation type, database configuration for the following items:

To find out which database items are associated with an outstation, display the References for that outstation (see Displaying a Database Item’s References).

You should ensure that each of the associated database items have valid, saved configuration and are In Service (if they are to function online), before downloading the data to an outstation (see Checking for Invalid Configuration, and see Placing an Item In Service).

To download configuration to an outstation:

WARNING

UNEXPECTED BEHAVIOR OF APPLICATION

Do not make further configuration changes to an outstation or any of its dependents while a download is in progress to that outstation. Performing such changes may result in partially updated or corrupt configuration being downloaded to the outstation, or configuration changes not being flagged for download.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
  1. Display the Database Bar (see Display an Explorer Bar).
  2. In the Database Bar, right-click on the required outstation.
    A context sensitive menu is displayed.
  3. Select the Download Configuration... option.
    The Download Configuration dialog box is displayed.

  4. Use the Download combo box to choose whether to download:
    • All Configuration—The complete configuration for that outstation and its associated components, is downloaded.
    • Changed Configuration Only—Only those configuration changes made to the outstation or its components since the last download, are sent to the outstation. This option is only available when supported by the driver and when such an option is applicable.
  5. Select the OK button to confirm the request.
    The specified configuration is downloaded to the outstation.

Disclaimer

ClearSCADA 2017 R3