Configure the Execution Settings for a Calculation Point

Use the fields within the Execution section of the Calculation tab to specify the specific triggers that will cause ClearSCADA to execute the calculation expression.

If you set a periodic trigger condition, you can view the next scheduled execution time in the point's status window. For more information, see Calculation Point Specific Status Attributes.

Examples for the Periodic trigger condition:

Example 1:

Interval: 1H, Offset: H+30M, Time Zone: Coordinated Universal Time (UTC).

ClearSCADA will execute the calculation expression every hour, at half past the hour UTC.

Example 2:

Interval: 1D, Offset: D+6H, Time Zone: Local Time with Daylight Saving Time.

ClearSCADA will execute the calculation expression daily at 6am local time, adjusted for Daylight Saving Time.

Further Information

Execute pick action: see Using Calculation Point Specific Actions.

Tags:see Tags in the ClearSCADA Guide to Expressions.

Hand Control: see Hand Control in the ClearSCADA Guide to ViewX and WebX Clients.

Internal Points: see Internal Points.

Override: see Override in the ClearSCADA Guide to Drivers.

Release Override:see Release Override in the ClearSCADA Guide to Drivers.

Accumulators: see Configuring Master Station Accumulators in the ClearSCADA Guide to Core Configuration.

Variables: see Using Variables to Store Data Values in the ClearSCADA Guide to Core Configuration.

Random Generators: see Understanding the Random Generator in the ClearSCADA Guide to the Random Generator.

Coordinated Universal Time: see Coordinated Universal Time in the ClearSCADA Guide to Core Configuration.

Daylight Saving Time: see Daylight Saving Time in the ClearSCADA Guide to Core Configuration.


Disclaimer

ClearSCADA 2017 R3