Display an X-Y-Z Plot in Design Mode

To edit an X-Y-Z Plot, you need to display it in Design mode. This mode provides access to the configuration features that enable you to change the appearance of the X-Y-Z Plot, add traces to the Plot, and so on.

To display an X-Y-Z Plot in Design mode:

  1. Log on to ViewX via a User Account that has the Configure Documents and Configure Database features enabled (on the User Form) and has the Configure permission for the X-Y-Z Plot (or its parent Group).
  2. Display the Database Bar (see Display an Explorer Bar).
  3. Expand the tree structure to locate the X-Y-Z Plot that you want to display in Design mode.
  4. Right-click on the X-Y-Z Plot in the Database Bar.
    A context-sensitive menu is displayed.
  5. Select the Edit X-Y-Z Plot option.
    The X-Y-Z Plot is displayed in Design mode..

Alternatively, you can display an X-Y-Z Plot in Design mode by performing one of the following:

Or:

Or:

  1. Display the X-Y-Z Plot in Run mode (see Display an X-Y-Z Plot in Run Mode).
  2. Perform one of the following:

    Or:

    • Select the Design Mode button on the Quick Access Toolbar.
    • Select the Design Mode command on the ViewX ribbon's Edit tab.

    Or:

  3. Right-click on the X-Y-Z Plot in a Queries List.
  4. Select the Edit option.

Disclaimer

ClearSCADA 2017 R3