Display the Schedule Times Window

This section applies to schedules other than Simple Schedules.

To display the Schedule Times window:

  1. Display the Schedule in Design Mode or Run mode.
  2. Right-click on the Schedule in the Document Display Area.
    A context-sensitive menu is displayed.
  3. Select the Schedule Times menu command from the relevant command group.
    The Schedule Times window is displayed, listing the trigger times, days, or dates (as applicable) for the events that are configured on that Schedule.

    The Format in which Schedule Times are Displayed varies, depending on the type of Schedule.

You can use the Schedule Times window to:


Disclaimer

Geo SCADA Expert 2020