Enable Unsolicited Alarm
            Associated with: DNP3 master outstations
The Enable Unsolicited Alarm attribute indicates whether the DNP3 ‘Enable Unsolicited’ message, sent by the Geo SCADA Expert DNP3 driver to enable unsolicited responses in the outstation, was successful.
The Geo SCADA Expert DNP3 driver will send the ‘Enable Unsolicited’ message if:
- You Enable Unsolicited Message Generation in the outstation
 - You Configure Virtual Terminal Support in the outstation
 - The Enable Unsolicited Events pick action is executed.
 
Possible States: Displays one of the Standard Alarm States.
Use the Unsolicited Event Reporting Status attribute to determine which unsolicited event classes are enabled in the outstation.