Points Used on EtherNet/IP Outstations

You use EtherNet/IP Points to read and/or write to items of data on Allen-Bradley controllers, using EtherNet/IP. You need to associate each tag on a controller with an EtherNet/IP Point of the relevant type in the Geo SCADA Expert database. This enables Geo SCADA Expert to perform the relevant processing of that tag's data in the Geo SCADA Expert database (for example, to monitor state changes, raise alarms, or execute controls).

The EtherNet/IP driver supports the point types that are listed below. You need to configure the points using the properties on the relevant EtherNet/IP Point Form.

You configure each point using the appropriate EtherNet/IP Point Form. The configuration Form contains many fields, organized into tabs. Most of these tabs contain properties that are common to points on many drivers (see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers).

Properties on the <Point Type> tab comprise:

The EtherNet/IP driver supports the controlling of points. EtherNet/IP points include a Control tab, which allows you to enable and configure the Control properties of points that operate as both an input and output. For more information, see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers. For analog points, also see Configure Analog Points.

In the Geo SCADA Expert documentation, we use the term ‘items of data’ to refer to ‘variables’ in Allen-Bradley controllers.

Further Information

Create a Point and Display a Point Form: see Create and Configure a Point in the Geo SCADA Expert Guide to Core Point Configuration.


Disclaimer

Geo SCADA Expert 2020