Configuring Digital Points
            The SCADAPack Modbus driver supports 1-, 2-, and 3-bit Digital Input points and Digital Output points.
Configure the properties for each Digital point using the fields on the SCADAPack Modbus Digital Input Point Form, or the SCADAPack Modbus Digital Output Point Form, as appropriate.
This section covers configuration of properties on the Digital Point tab of both SCADAPack Modbus Digital Point Forms, and the properties on the Control tab for Digital Output points. The properties on other tabs are common to points on many advance drivers (see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers).
Use the Digital Point tab to:
- Configure Common Point Properties
 - Specify the Point State Properties
 - Define Override Properties (see Define whether a Digital Point can be Overridden in the Geo SCADA Expert Guide to Core Point Configuration)
 - Define Trend Properties (see Define a Digital Point’s Trend Settings in the Geo SCADA Expert Guide to Core Point Configuration)
 - Specify the Logged Data Properties.
 
For SCADAPack Modbus Digital Output Points there are two additional tabs: a Control Tab and a Control Checks tab.
Use the Control tab to:
- Configure the Control Actions (see Define the Control Settings for a Digital Output Point in the Geo SCADA Expert Guide to Core Point Configuration)
 - Specify whether any Controllers are given Scanning Priority whenever a Control Action is Issued (see Promoting Scanning of Outstations Associated with Controls in the Geo SCADA Expert Guide to Core Point Configuration)
 - Specify the Type of Control Operation
 - Specify Whether to Restore the Control Value Following a Cold Reset
 - Specify Whether to Update the Point Value Immediately Following a Control.
 
You can optionally use the Control Checks tab to configure the Control Checks settings (see Configuring Control Checks Settings in the Geo SCADA Expert Guide to Core Point Configuration).