Actions Associated with Slave Outstations on Advanced Drivers
            With most advanced driver setups, Geo SCADA Expert is the SCADA master. Some drivers support slave functionality, whereby the Geo SCADA Expert system acts as an outstation or similar device and reports any data changes back to its SCADA master (see Master-Slave Communications). On systems on which Geo SCADA Expert is a slave, the Slave outstations support a combination of these actions:
- Acknowledge Alarms
 - Acknowledge with Comment
 - Alarm Response
 - Cancel Promoted Dial Out—(PSTN Slave outstations)
 - Close Line—(PSTN Slave outstations)
 - Disable Alarms
 - Disable Outstation
 - Enable Alarms
 - Enable Outstation
 - Extend Line—(PSTN Slave outstations)
 - One Shot—(PSTN Slave outstations)
 - Open Line—(PSTN Slave outstations)
 - Preferred Channel—(PSTN Slave outstations)
 - Promote Dial Out—(PSTN Slave outstations)
 - Release Exclusive Control—(Systems on which Exclusive Control is enabled)
 - Remove Alarms
 - Remove with Comment
 - Reset Call Statistics—(PSTN Slave outstations)
 - Reset Comms Statistics
 - Reset Point Statistics
 - Take Complete Exclusive Control—(Systems on which Exclusive Control is enabled)
 - Take Partial Exclusive Control—(Systems on which Exclusive Control is enabled)
 - Unacknowledge Alarms
 - Unacknowledge with Comment.
 
                            
Further Information
‘Core’ pick actions that are common to many database items: see Object Menu Options in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients.
For information on any slave outstation-specific actions that are not listed above, see the relevant driver guide.