Introduction to the ODBC Driver

This driver is a simple driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

Intended Audience

This guide is intended for all levels of user:

Document Scope

This guide explains features that are specific to the Geo SCADA Expert ODBC Driver. This driver has been produced by Schneider Electric to run on the servers on a Geo SCADA Expert system, and should not be confused with the WindowsTM ODBC driver that is often supplied with WindowsTM software. In this guide, the Geo SCADA Expert ODBC driver is generally referred to as the ODBC driver.

The Geo SCADA Expert ODBC Driver allows point data to be transferred from another database into the Geo SCADA Expert database, using Open DataBase Connectivity (ODBC) data transfer standards (see Using ODBC to Access the Geo SCADA Expert Database). The driver performs the necessary conversions to enable the data to be transferred between the source and destination databases. This is dependent on:

ODBC can be used to transfer data between a Geo SCADA Expert database and, for example, Oracle, Access, Excel, dBase or an SQL server.

In Geo SCADA Expert, you can write an ODBC Query using SQL that allows a block of data to be located and retrieved from the other application’s database. As with other ODBC drivers, Geo SCADA Expert’s ODBC driver converts that query into a request that can be recognized by the other application’s database management system. The other application can then perform the requested data transfer.

You use OBDC points in Geo SCADA Expert to extract data from the data table that is produced as a result of the ODBC query request. If timestamps are to be extracted, these should be in UTC.

Given the required Write access privileges, you can also replace or insert an individual value within another application’s database, by sending a point control to that application. Within Geo SCADA Expert, you enter the SQL Query code that defines the location of the data in the other application’s database and the specifies the data that is to be replaced or inserted. The actual value that is to be sent to the other application’s database, is specified when the control is requested.

The ODBC documentation explains how to configure ODBC-specific features and items in the Geo SCADA Expert database (see Configuration Order). It also explains the driver-specific features that are of interest to operators, such as:

and driver-specific aspects that may be of interest to system administrators and engineers when investigating unexpected system behavior:

Use the documentation along with the Geo SCADA Expert Guide to Simple Drivers and the core documentation when configuring ODBC features on your system.

For other applications to access the Geo SCADA Expert database using ODBC, the appropriate Data Access components have to be installed as part of the Geo SCADA Expert installation process. For more information, see Third Party ODBC Client - System Connections in the Geo SCADA Expert Guide to Client Administration.

For information on exporting Crystal Reports in ODBC format, see the Geo SCADA Expert Crystal Reports documentation.


Disclaimer

Geo SCADA Expert 2019