Status Attributes Associated with Slave Outstations on Advanced Drivers

With most advanced driver setups, Geo SCADA Expert is the SCADA master. However, some drivers support slave functionality, whereby the Geo SCADA Expert system acts as an outstation or similar device and reports any data changes back to its SCADA master (see Master-Slave Communications).

On systems on which Geo SCADA Expert is a slave, the driver’s Slave outstations support a combination of these status attributes:

For information on slave outstation status attributes that are not listed above, see the driver-specific documentation.


Disclaimer

Geo SCADA Expert 2021