Information

The General branch of the Server Status Tool includes an Information category. The category provides status information about the current status of the server's hardware and software. When applicable, it also displays warnings to highlight potential issues with system security or database usage.

The Information category provides a variety of information about the server, including:

Warnings Shown in Highlighted Text

When applicable, warnings are displayed to highlight potential issues with system security or database usage. These are shown towards the top of the Information category.

 


Disclaimer

Geo SCADA Expert 2022