Display Property Changes

Associated with: All database items, but only when the Configuration Changes Auditing feature is enabled (see Configuration Changes Auditing).

Select this option to view a List of the configuration changes made to an item. For more information, see Display a List of Property Changes.

With a ViewX client on a Multi-Monitor Setup, you may be able to select the name of the Window Container in which to display or edit a document. Each Window Container displays on a particular monitor by default. Such options are only available when you select certain Display... or Edit... pick actions from the Database Bar or Operator Documents Bar. For more information, see Ability to Specify the Window Container in which to Display or Edit a Document.


Disclaimer

Geo SCADA Expert 2022