Using OPC Time Formats

Use OPC time formats for entering dates and times in ClearSCADA. The formats are based on the standards that are defined by the OPC Foundation. The formats that you need to use vary, depending on the type of time or date. Within ClearSCADA you can enter and display these types of dates and times:

The relevant sections in the ClearSCADA documentation indicate which format you should be using to specify a time or date.

Further Information

OPC Foundation Standards: See www.opcfoundation.org

Time Zone Support in ClearSCADA.


Disclaimer

ClearSCADA 2017 R3