Promote Dial Out

Associated with: Outstation sets; PSTN outstations or outstations with PSTN fallback; Slave PSTN outstations

This pick action is only available for an outstation or set on which:

Use the Promote Dial Out pick action to temporarily increase the rate at which ClearSCADA retrieves data from one or more outstations (see Temporarily Increasing the Frequency with which an Outstation is Called in the ClearSCADA Guide to Advanced Drivers). When this pick action is used on an outstation, ClearSCADA sends One Shot requests to that particular outstation at a promoted rate, for the duration of the promotion. When executed on a set, ClearSCADA sends One Shot requests at a promoted rate to each of the outstations on that set. For more information on the order in which ClearSCADA contacts the outstations in a set, see One Shot.

Select the pick action to display the Promote Dial Out window.

Use the fields and check box to specify the required promotion:

The Promoted Dial Out defaults for the outstations on your system are specified using the ClearSCADA Server Configuration Tool (see Define the Default Promoted Dial Out Settings in the ClearSCADA Guide to Server Administration.

The Dial Out Promoted status attribute indicates whether dial-outs are promoted on a set or outstation.

Also see Cancel Promoted Dial Out.


Disclaimer

ClearSCADA 2017 R3