Pre-Configured Trends and Ad Hoc Trends

ClearSCADA supports these different types of Trend:

The trace(s) on Trends may display either:

The configuration of the point object determines if the ‘standard’ ad hoc Trend will display Raw Historic or Processed Historic data (see Defining Historic Details for a Point).

To create and configure Trends in ViewX, you need to log on via a User Account that has the Configure permission. For more information, see Configuring Trends, and Using TrendSpec to Produce Ad Hoc Trends.

To view a Trend, you need to access the Trend via a ViewX or WebX client (see Using Trends).

Further Information

Raw Historic Data on Trends

Processed Historic Data on Trends


Disclaimer

ClearSCADA 2017 R3