Liquid Flow Run Properties
For a Liquid Flow Run use the fields on the Liquid tab of the Flow Run Form to Configure the Flow Run Properties.
You can configure these properties directly in Geo SCADA Expert, or read the configuration into the Geo SCADA Expert database (see Configure or Read the Flow Run Configuration).
With the properties listed below, you can either Configure or Read the Flow Run Configuration.
- Density Properties (Liquid Flow Run)—Use this section to define the properties for configuring density input scaling.
- Water Cut Properties (Liquid Flow Run)—Use this section to define how much of the total liquid is oil or water and how that quantity is defined as a percentage of how much water is in the liquid.
- Liquids Properties (Liquid Flow Run)—Use this section to configure common liquid flow run properties.
- Two-Phase Detection (Liquid Flow Run)—Use this section to specify whether the flow calculation uses two-phase detection, and if so, the properties that relate to the type of detection being used.
- Pressure Compensation Properties (Liquid Flow Run)—Use this section to define whether the flow calculation includes pressure compensation. (The properties are supported by Realflo version 6.95 onwards.)