Actions Associated with Slave Outstations on Advanced Drivers

With most advanced driver setups, ClearSCADA is the SCADA master. Some drivers support slave functionality, whereby the ClearSCADA system acts as an outstation or similar device and reports any data changes back to its SCADA master (see Master-Slave Communications). On systems on which ClearSCADA is a slave, the Slave outstations support a combination of these actions:

Further Information

‘Core’ pick actions that are common to many database items: see Object Menu Options in the ClearSCADA Guide to ViewX and WebX Clients.

For information on any slave outstation-specific actions that are not listed above, see the relevant driver guide.


Disclaimer

ClearSCADA 2017 R2