Actions Associated with Pulse Actions
Pulse actions support a combination of these actions:
- Abort Pulse
- Acknowledge Alarms
- Acknowledge with Comment
- Alarm Response
- Cancel Control—(Pulse Actions on simple drivers)
- Cancel Queued Request—(Pulse Actions on advanced drivers)
- Control
- Disable Alarms
- Disable Controls
- Disable Point
- Enable Alarms
- Enable Controls
- Enable Point
- Inching—(Pulse actions that support user-definable control periods)
- Release Exclusive Control—(Systems on which Exclusive Control is enabled)
- Remove Alarms
- Remove with Comment
- Take Complete Exclusive Control—(Systems on which Exclusive Control is enabled)
- Take Partial Exclusive Control—(Systems on which Exclusive Control is enabled)
- Unacknowledge Alarms
- Unacknowledge with Comment.
Further Information
‘Core’ pick actions that are common to many database items: see Object Menu Options in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients.
For information on any pulse-specific actions that are not listed above, see the relevant driver guide.