Status Attributes Associated with Outstations on Advanced Drivers
Slave outstations have a subset of these attributes (see Status Attributes Associated with Slave Outstations on Advanced Drivers).
The outstations on advanced drivers support a combination of these status attributes:
- Id
- Full Name
- Type
- Position
- Created—(New outstations only)
- Last Modified
- Configuration Change CRC—(Only displayed if this feature is enabled on your system)
- Exclusive Control User—(Only outstations that are under Exclusive Control)
- Queued Request—(Outstations on which pick action requests are queued)
- Alarm State
- Alarm Last Updated
- Dial In Overactive Alarm—(Outstations on which Dial In Overactive is enabled)
- PSTN Test Alarm
- Comms State Alarm
- Channel State Alarm
- Protocol Alarm—(Displayed when supported by the driver)
- Download Config Alarm—(Displayed when supported by the driver)
- Scanner Command Alarm
- Alarm Count
- Suppression Status—(Outstations on which Alarm Suppression is configured)
- Suppressing Parent—(Outstations on which alarms are currently suppressed)
- Source Name
- Source
- Network—(Network-connected outstations only)
- State
- Last Updated
- Quality
- Current Channel
- Scanning—(Direct outstations, displayed only while scanning is promoted)
- Comms Statistics
- Last Polled
- Point Statistics
- Telephone Number—(PSTN outstations, or outstations on which PSTN fallback is enabled)
- Preferred Channel—(Outstations for which a preferred PSTN channel is specified)
- Incoming Calls—(PSTN outstations, or outstations that support PSTN fallback)
- Last Good Incoming Call—(PSTN outstations, or outstations that support PSTN fallback)
- Last Incoming Call Lost Comms—(PSTN outstations, or outstations that support PSTN fallback)
- Outgoing Calls—(PSTN outstations, or outstations that support PSTN fallback)
- Last Good Outgoing Call—(PSTN outstations, or outstations that support PSTN fallback)
- Last Outgoing Call Lost Comms—(PSTN outstations, or outstations that support PSTN fallback)
- Last Outgoing Call Not Established—(PSTN outstations, or outstations that support PSTN fallback)
- Dial In Overactive—(Outstations on which the Dial Out feature is enabled)
- Dial Out Promoted—(Outstations on which the Dial Out feature is enabled)
- Switching—(Shared outstations that are ‘Independent’).
For information on outstation status attributes that are not listed above, see the driver-specific documentation.