Status Attributes Associated with Points
Pulse actions have a subset of these attributes (see Status Attributes Associated with Pulse Actions).
Points on many drivers support a combination of these status attributes:
- Id
- Full Name
- Type
- Position
- Created—(New points only)
- Last Modified
- Configuration Change CRC—(Only displayed if this feature is enabled on your system)
- Exclusive Control User—(Only points that are under Exclusive Control)
- Queued Request—(Output points for which pick action requests are queued)
- Alarm State
- Alarm Last Updated
- No Change Alarm—(Points on which the No Change feature is enabled)
- Control Alarm—(Output points only)
- State Alarm
- Alarm Count
- Suppression Status—(Points on which Alarm Suppression is configured)
- Suppressing Parent—(Points on which alarms are currently suppressed)
- Source Name
- Source
- Parent Point—(Points that have a parent point)
- Current Value
- Current State
- Last Updated
- Current Quality
- Current Status
- Override—(Where supported and enabled for a point)
- Put Aside Value—(Only displayed while an Override is in force)
- Put Aside State—(Only displayed while an Override is in force)
- Put Aside Last Updated—(Only displayed while an Override is in force)
- Put Aside Quality—(Only displayed while an Override is in force)
- Put Aside Status—(Only displayed while an Override is in force)
- Previous Update Value
- Previous Update State
- Previously Updated
- Previous Update Quality
- Previous Update Status
- Previous State
- State Change Value
- Last Changed State
- State Change Quality
- State Change Status
- Process Count
- Logged Value—(Points that have logged data)
- Logged State—(Points that have logged data)
- Logged Time—(Points that have logged data)
- Logged Quality—(Points that have logged data)
- Logged Status—(Points that have logged data)
- End of Period Value—(Points that have end of period data)
- End of Period State—(Points that have end of period data)
- End of Period Time—(Points that have end of period data)
- End of Period Quality—(Points that have end of period data)
- End of Period Status—(Points that have end of period data)
- Previous End of Period Value—(Points that have end of period data)
- Previous End of Period State—(Points that have end of period data)
- Previous End of Period Time—(Points that have end of period data)
- Previous End of Period Quality—(Points that have end of period data)
- Previous End of Period Status—(Points that have end of period data)
- Controls—(Output points only)
- Alarm Limits—(Analog and Counter-type points for which the limits are currently tuned)
- Current M/S State—(Analog points on which Master Station Alarm Limits are used)
- M/S Alarm Limits—(Analog points on which one or more of the Master Station Alarm Limits are tuned)
- Last Execution—(Calculation points only)
- Last Executed—(Calculation points only)
- Next Execution—(Calculation points only).
- Control Feedback Point—(only displayed if control feedback is enabled and there is a feedback check point associated with the point)
- Waiting For Feedback—(only displayed if control feedback is enabled and there is a feedback check point associated with the point)
- Last Feedback Timed Out—(only displayed if control feedback is enabled and there is a feedback check point associated with the point)
- Uncommanded Change Point—(only displayed if uncommanded change detection is enabled and there is an uncommanded change check point associated with the point)
- Has Uncommanded Change(only displayed if uncommanded change detection is enabled and there is an uncommanded change check point associated with the point).
For information on point status attributes that are not listed above, see the driver-specific documentation.