Points Used on Sofrel Outstations

Sofrel outstations support a combination of these point types:

You need to configure one point of the appropriate type per point at an outstation. You configure the properties of each point using the appropriate Sofrel Point Form.

This section covers the configuration of properties that are common to many Sofrel points. It includes information on how to:

For Sofrel Analog Output Points and Sofrel Digital Output Points, it also explains how to:

Minimum Configuration

For each point, you need to specify the following features on the appropriately named <Point Type> tab, then put the point In Service and save the configuration:

If the point is an output point, you need to:

If you want point data to be stored historically, you also need to:

These are the minimum requirements and, when configured, will result in a functional point that uses the default settings.

For general information on creating a point and displaying a Point Form, see Configuring a Point.


Disclaimer

Geo SCADA Expert 2022