Welcome to the Client Administration Guide

Welcome to the ClearSCADA Guide to Client Administration. This guide is designed to help you understand how ClearSCADA clients (ViewX, WebX, XML, and Third Party OPC) connect to your ClearSCADA system and provides information on client specific settings and features.

Intended Audience

The ClearSCADA Guide to Client Administration is aimed at administrator level users who are responsible for the initial set-up of client connections and settings. For information about the various ViewX and WebX features, you should refer to the ClearSCADA Guide to ViewX and WebX Clients.

Document Scope

This guide explains how ClearSCADA clients (ViewX, WebX, XML, and Third Party OPC) connect to your ClearSCADA system and provides information on client-specific settings and features.

In this guide, you will find information on:

Further Information

Client PC requirements: see Client PC Requirements in the ClearSCADA Installation Guide.


Disclaimer

ClearSCADA 2017 R3