Understand the WebX Interface

ATTENTION: This topic relates to the deprecated Original WebX client that is supported by this and previous versions of ClearSCADA. For information about the WebX client that is supported by ClearSCADA 2015 R1 onwards, for which the web server is hosted using IIS, click here.

The WebX interface consists of two parts:

The WebX interface navigation bar contains a number of buttons that you use to access your system. You select a button to access the next page or display for that particular feature. The buttons that are shown vary, depending on the access assigned to your user account, but comprise a combination of the following:


Disclaimer

ClearSCADA 2017 R3