Display a 'File' Type Object in Run Mode
A 'file' type object is a database item for which you configure various properties using an Editor. Geo SCADA Expert supports various 'file' type objects
You display a 'file' type object in Run mode to access that object's operational features (see Run Mode).
To display a 'file' type object in Run mode, you need to log on via a User Account that has the Operate feature enabled (on the User Form) and has the Read and Browse permissions for the 'file' type object (or its parent Group). See a system administrator if your User Account does not appear to provide the required level of access.
To display a 'file' type object in Run mode, you typically select the relevant Display pick action or menu option:
- Log on to ViewX or Virtual ViewX via a suitable User Account (see above).
- Display the Database Bar (see Display an Explorer Bar).
- Expand the tree-structure in the Database Bar to locate the 'file' type object that you want to display.
- Right-click on the required 'file' type object in the Database Bar.
A context-sensitive menu is displayed. - Select the relevant Display pick action. (For example, if the 'file' type object is a Trend, select the Display Trend pick action.)
The selected object is displayed in Run mode.
Alternatively, use one of the following means of displaying a 'file' type object in Run mode:
- Double-click on the 'file' type object in the Database Bar (if your User Account does not have the Double Click Edits Documents feature enabled).
Or:
- Display the 'file' type object on, or from, a suitably configured Mimic.
Or:
- Select an animated representation of the 'file' type object on a suitably configured Mimic. (Providing that the animated representation is associated with the object's Pick Action Menu and provides access to the relevant menu option.)
- Select the Display option.
Or:
- Right-click on the 'file' type object in a Queries List.
- Select the Display option.
Or:
- If your User Account provides access to Favorites, you can display a 'file' type object that you have previously added to your Favorites list. For more information, see Use the Favorites Bar to Access your Favorites in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients.
Or:
- Display the 'file' type object in Design mode (see Display a File Type Object in Design Mode). (Providing that your User Account's settings enable you to access the 'file' type object in Design mode.)
- Perform one of the following:
- Deselect the Design Mode button
on the Quick Access Toolbar.Or:
- Deselect the Design Mode command
on the ViewX ribbon's Edit tab.
- Deselect the Design Mode button
Although Logic programs are 'file' type objects, they do not have a 'Display' pick action to enable them to be viewed in Run mode. Instead, you use the Execute pick action when you want to trigger the Logic program manually. For more information, see Using Actions Associated with Logic Programs in the Geo SCADA Expert Guide to Logic.
With a ViewX client on a Multi-Monitor Setup, you may be able to select the name of the Window Container in which to display or edit a document. Each Window Container displays on a particular monitor by default. Such options are only available when you select certain Display... or Edit... pick actions from the Database Bar or Operator Documents Bar. For more information, see Ability to Specify the Window Container in which to Display or Edit a Document.
Further Information
User Accounts and security permissions: see Database Security.
Working with a 'file' type object in Run mode: see the relevant object-specific section or guide. (For example, for information on working with Trends, see the Geo SCADA Expert Guide to Trends.)
Display and operate 'file' type objects on an Original WebX client: see Use the WebX Interface.