Actions Associated with Outstations on Advanced Drivers

Slave outstations support a subset of these actions (see Actions Associated with Slave Outstations on Advanced Drivers).

The outstations on advanced drivers support a combination of these actions:

The options Delete Interface Event, Log Interface Event, Modify Interface Event, Refresh Alarms, and Reprioritize Alarms are also available from the Edit Action, Edit Method, and Pick Action Configuration windows. These options are methods, not pick actions, and are purely for use with the Automation Interface. For information, see the database Schema.

Further Information

‘Core’ pick actions that are common to many database items: see Object Menu Options in the ClearSCADA Guide to ViewX and WebX Clients.

For information on any outstation-specific actions that are not listed above, see the relevant driver guide.


Disclaimer

ClearSCADA 2017 R2