List of Status Attributes

The subsections within this section summarize the status attributes that are common to items on many drivers. Be aware that some attributes are only displayed once ClearSCADA has been in communications with a device and has been able to retrieve the relevant information.

The subsections within this section are arranged in order, by status attribute name.

You can also display a list of the status attributes that are commonly associated with a particular driver item, such as a channel, or scanner (see Status Attributes that are Common to Many Drivers).

For information on accessing an item’s Status display, see Status Displays in the ClearSCADA Guide to ViewX and WebX Clients.

These status attributes are common to items on many drivers:

For information on any status attributes that are not listed above, see the driver-specific documentation.


Disclaimer

ClearSCADA 2017 R2