Server Status Categories
The Server Status Tool provides status information that is organized into the following categories:
- General—Please refer to General System Status Information
- Database—Please refer to Database Status Information
- Server—Please refer to Server Status Information
- Standby—Please refer to Standby Status Information
- Historic—Please refer to Historic Status Information
- Query Processor—Please refer to Query Processor Status Information
- OPC—Please refer to OPC Status Information
- .NET Tags — Reserved for use with future client applications.
- DA Groups
- DA Items
- HDA Items
- XML-DA Items
- XML-DA Subscriptions
- Web—Please refer to Original WebX Status Information
If you select the folder for a branch of status categories (rather than select a specific category from within that branch), the tool will display the status information that relates to the first category in that branch. For example, if you select the folder for the Server branch, the tool will display the status data for the Advise Threads category (as that is the first category in the Server branch).